System reference
Gripper in use at the Föhl company
Gripper | System solutions
          Task & Solution
        
For Föhl GmbH + Co KG, the Zimmer Group has supplied system solutions for a robot cell in which zinc die-cast gearbox housings for awning motors are handled. A turning station was designed for this purpose, into which the robot inserts the two workpieces as it has removed them from the deburring press. Two pneumatic parallel grippers of type GPP5006N serve as workpiece holders in the turning station.
      Built-in standard components